LTE employs a new network architecture made up of multiple Evolved Packet Cores (EPCs) that communicate with each other and with evolved universal terrestrial radio access network base stations (eNBs). Each EPC contains a Mobile Management Entity (MME) and a System Architecture Evolution Gateway (SAE). The eNB stations communicate with the EPCs, with each other, and with user equipment (UE).
Click Downlink in the tree view to open the Downlink node. The Downlink node enables you to set parameters of the cell, reference signal, and synchronization signals.
The Downlink parameters are described in Cell Parameters (Basic LTE-A FDD Downlink), Reference Signal (Basic LTE-A FDD Downlink), Synchronization Signals (Basic LTE-A FDD Downlink), and Channel State Information Reference Signal Parameters (Basic LTE-A FDD Downlink).
|
Downlink |
|---|
Click
the button
to access a
dialog box
+ from which you can select a base channel configuration.
Click
the Test Model Wizard button
to access a dialog box
from which you can select a test model configuration.